Reports a synchronous signal.
Include
<signal.h>
Prototype
int raise(int sig);
Argument
sig |
Return Value
Returns a 0 if successful; otherwise, returns a non-zero value.
Remarks
raise
sends the signal identified by sig
to the executing
program.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <signal.h>
#include <stdlib.h>
#include <stdio.h>
#include <xc.h>
void __attribute__((interrupt(auto_psv))) _MathError(void)
{
raise(SIGILL);
INTCON1bits.MATHERR = 0;
}
void illegalinsn(int idsig)
{
printf("Illegal instruction executed\n");
exit(1);
}
int main(void)
{
int x, y;
div_t z;
signal(SIGILL, illegalinsn);
x = 7;
y = 0;
z = div(x, y);
printf("Program never reaches here");
}
Example Output
Illegal instruction executed
Example Explanation
This example requires the linker script, p30f6014.gld
. There are three
parts to this example.
First, an interrupt handler is written for the interrupt vector,
_MathError
, to handle a math error by sending an illegal
instruction, signal (SIGILL)
, to the executing program. The last
statement in the interrupt handler clears the exception flag.
Second, the function illegalinsn
will print an error message and call
exit
.
Third, in main
, signal (SIGILL, illegalinsn)
sets the
handler for SIGILL
to the function illegalinsn
.
When a math error occurs due to a divide by zero, the _MathError
interrupt vector is called, which in turn will raise a signal that will call the handler
function for SIGILL
: the function illegalinsn
. Thus,
error messages are printed and the program is terminated.