Test for an alphanumeric character.
Include
<ctype.h>
Prototype
int isalnum(int c);
Argument
c
|
Return Value
Returns a non-zero integer value if the character, c
, is
alphanumeric; otherwise, returns a zero.
Remarks
Alphanumeric characters are included within the ranges
'A'
-'Z'
, 'a'
-'z'
or
'0'
-'9'
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = '3';
if (isalnum(ch))
printf("3 is an alphanumeric\n");
else
printf("3 is NOT an alphanumeric\n");
ch = '#';
if (isalnum(ch))
printf("# is an alphanumeric\n");
else
printf("# is NOT an alphanumeric\n");
}
Example Output
3 is an alphanumeric
# is NOT an alphanumeric