Converts calendar time to time structure expressed as Universal Time Coordinated (UTC) also known as Greenwich Mean Time (GMT).
Include
<time.h>
Prototype
struct tm *gmtime(const time_t *tod);
Argument
tod |
Return Value
Returns the address of the time structure.
Remarks
This function breaks down the tod
value into the time
structure of type tm
. By default, the compiler returns the time as
instruction cycles. With this default, gmtime
and
localtime
will be equivalent, except gmtime
will
return tm_isdst
(Daylight Savings Time flag) as zero to indicate that
Daylight Savings Time is not in effect.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <time.h>
#include <stdio.h>
int main(void)
{
time_t timer;
struct tm *newtime;
timer = 1066668182; /* Mon Oct 20 16:43:02 2003 */
newtime = gmtime(&timer);
printf("UTC time = %s\n", asctime(newtime));
}
Example Output
UTC time = Mon Oct 20 16:43:02 2003