Copies a va_list
object.
Include
<stdarg.h>
Prototype
void va_copy(va_list dest, va_list src);
Arguments
dest | va_list object to be initialized |
src | va_list object to copy |
Remarks
The function copies the src
object into dest
, such that
the state of dest
will reflect any call made to
va_start
to intialize src
as well as the same
sequence of va_arg
macro calls that modified src
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
#include <stdarg.h>
#include <limits.h>
/* print values as a percentage of the maximum value
* list ends with 0 value
*/
void PrintAsPercent(int first, ...)
{
char * buffer;
int val = first;
int valMax = INT_MIN;
va_list vl_parse, vl_print;
va_start(vl_parse, first);
/* copy, after having called va_start */
va_copy(vl_print, vl_parse);
/* find the largest value */
while(val != 0) {
val = va_arg(vl_parse, int);
if(val > valMax)
valMax = val;
}
va_end(vl_parse);
/* va_start not necessary with va_print */
val = first;
while(val != 0) {
printf("%d%% ", val*100/valMax);
val = va_arg(vl_print, int);
}
va_end(vl_print);
printf("\n");
}
int main(void)
{
PrintAsPercent(10, 23, 156, 42, 88, 0);
}
Example Output
6% 14% 100% 26% 56%