Calculates the absolute value of a long double precision floating-point value.
Include
<math.h>
Prototype
long double fabsl(long double x);
Argument
x |
Return Value
Returns the absolute value of x
. A negative number is
returned as positive; a positive number is unchanged.
Remarks
No domain or range error will occur.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x, y;
x = 1.75;
y = fabsl(x);
printf("The absolute value of %Lf is %Lf\n", x, y);
x = -1.5;
y = fabsl(x);
printf("The absolute value of %Lf is %Lf\n", x, y);
}
Example Output
The absolute value of 1.750000 is 1.750000
The absolute value of -1.500000 is 1.500000