Returns the long double precision floating-point argument rounded to an integer value.
Include
<math.h>
Prototype
long int lroundl(long double x);
Argument
x |
Return Value
Returns the value of x
rounded to the nearest integer value, always
rounding midway cases away from zero. The rounded integer is returned as a
long
integer value.
Remarks
The value returned is unspecified should the rounded value fall outside the range of the return type.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x;
long int y;
x = 10.103;
y = lroundl(x);
printf("The nearest integer value to %Lf is %ld\n", x, y);
x = 10.5;
y = lroundl(x);
printf("The nearest integer value to %Lf is %ld\n", x, y);
}
Example Output
The nearest integer value to 10.103000 is 10
The nearest integer value to 10.500000 is 11