The MCC configuration was made for PIC16F1779 and Curiosity HPC development
board, but the transceiver solution can be implemented on any 8-bit MCU that has a CLC, an
EUSART, a TMR with HLT and two TMRs with gate control. The configuration is based on a system
clock of 4 MHz. All the required peripherals are available for configuration in MCC.
The tools versions used are:
- MPLAB X IDE v4.15
- XC8 v1.45
- MCC Plugin v3.55.1
- MCC Core v4.45
- MCC 8-bit Library v1.65.2
These are the configuration steps:
- 1.Start MPLAB X and create a new project for
PIC16F1779.
- 2.Open MCC.
- 3.In System Module, change internal
clock to 4MHz_HF and disable PLL by unchecking PLL Enabled checkbox.
Figure 1. System Module
- 4.From Device Resources → Peripherals
shown in Figure 2, select a CLC, an EUSART and three Timer
modules.
Figure 2. Peripherals Selection
- 5.The CLC must act like an XOR gate,
with its input signals coming from EUSART, as shown in Figure 3; the demo is using CLC4:
- Enable CLC → uncheck box
- Mode → OR-XOR
- Configure the first signal to be the
Clock (CK) channel from the EUSART module, and enable the connection to the first or the
second gate
- Configure another signal to be the Data
(DT) channel from the EUSART module, and enable the connection to the third or the
fourth gate
- Negate the Data signal by pressing on
the top of the gate to which it was assigned
Figure 3. CLC4 Configurations
- 6.The EUSART must be configured as
synchronous and with a baud rate of 1200, as indicated in Figure 4, to satisfy the DALI-2 requirements, and also the EUSART
interrupts must be enabled:
- Mode → Synchronous
- Sync Mode → master
- Baud Rate → 1200
- Enable EUSART Interrupts → Check
Figure 4. EUSART Configuration
- 7.A Timer was used to generate an
interrupt after the end of the transmission, leaving the communication channel into an Idle
state. The demo is using TMR8 and the configuration is illustrated in Figure 5:
- Enable Timer → uncheck box
- Clock Source → FOSC/4
- Postscaler → 1:1
- Prescaler → 1:32
- Timer Period → 416 μs
- Enable Timer Interrupt → check box
- Callback Function Rate → 416 μs
Figure 5. TMR8 Configuration
Note: TMR8 is also used by the
decoder, which will modify the prescaler and Period values. There is no
problem, since the decoder and the encoder will never be both active at the same time.
When disabled, the decoder will revert the Period to the value set in MCC. The
encoder will set the prescaler back to 1:32 when needed.
- 8.Additionally, the decoder uses two
timers with gate control for measuring the actual baud rate of the received
signal and adjust the EUSART baud rate accordingly. The demo is using TMR1 and
TMR5 for this, and the configurations are illustrated in Figure 6, respectively Figure 7:
- Enable Synchronization → uncheck
box
- Enable Gate → check box
- Enable Gate Toggle → check box (just
for TMR1)
- Enable Gate Single-Pulse mode → check
box
- Gate Polarity → high
Figure 6. TMR1 Configuration
Figure 7. TMR5 Configuration
- 9.In Pin Manager from Figure 8, the user must select the CLC module output pin,
buttons input pins, EUSART DT pin, LEDs output pins, TMR1 and TMR5 gate
pins and TMR8 input pin:
- CLC4OUT → output on Port RD0; disable
Analog
- EUSART DT → connect to Port RB5
- Pin Module → input Port RB4; rename the
pin to S1; enable Weak Pull-Up
- Pin Module → input Port RC5; rename the
pin to S2; enable Weak Pull-Up
- Pin Module → output Port RA4; rename
the pin to LED_D2; disable Analog
- Pin Module → output Port RA5; rename
the pin to LED_D3; disable Analog
- Pin Module → output Port RA6; rename
the pin to LED_D4
- Pin Module → output Port RA7; rename
the pin to LED_D5
- TMR1 T1G → input from Port RB5
- TMR5 T5G → input from Port RB5
- TMR8 T8IN → input from Port RB5
Figure 8. Pin Manager Configurations
- 10.The configurations for Manchester
transceiver were made, so the Generate button can be pressed.