Figure 1 shows the internal architecture of the MSS GPIO block. GPIOs and MSS peripherals, such as MMUART, SPI, and I2C, can be routed to MSIO pads or to the FPGA fabric through I/O multiplexers (MUXes), as shown in the figure.
The MSS GPIO block contains the following:
When a GPIO is configured in Input mode, the GPIO input is passed through two flip-flop synchronizer and latched into the GPIO_IN register. The GPIO_IN register value is read through the APB bus and is accessible to the processor or fabric master. The inputs to GPIO0 and GPIO1 are from MSIOs. The inputs to GPIO2 are from the fabric.
The GPIO_IN register output can also be used as an interrupt to the processor. This can be configured as an edge triggered (on rising edge, falling edge, or both edges) or as a level sensitive (active-low or active-high) interrupt. The interrupt is latched in the GPIO_INTR register and is accessible through the APB bus.
In Edge-sensitive mode, GPIO_INTR register is cleared either by disabling the interrupt or writing a Logic 1 through the APB interface. If an edge and GPIO_INTR clearing through the APB occurs simultaneously, the edge has higher priority.
When the GPIO is configured in an Output mode, the output value can be configured using the APB bus and is accessible to the processor or fabric Master. GPIO0 and GPIO1 outputs are available to MSIOs. GPIO2 outputs are available to the fabric.