Data trace on a slave port involves the following steps:
- 1.Programming the design on the PolarFire SoC device.
- 2.Running the firmware to create traffic on S1 slave port using SoftConsole.
- 3.Discovering Trace modules using SoftConsole.
- 4.Configuring the AXI Monitor 0 bus monitor using SoftConsole.
- 5.Running and monitoring the AXI(64) trace data using SoftConsole.
Note: The monitored trace data must match with the data sent/received on S1 slave.
The following figure shows the required trace modules and the flow involved in AXI Switch data trace.
Figure 1. AXI Switch Data Trace
Note: The configuration of AXI Monitor 0 involves setting GPIO_0 to enable trace on the S1 port connected to FIC0.