The AXI switch uses a QoS scheme to control priorities in the switch and the DDR controller. The QoS is a 4-bit value and a higher QoS value represents a higher priority.
Each master generates a QoS as listed in the following table.
Port | Master | Master Directly supports QoS (Yes/No) | QoS Source |
---|---|---|---|
1 | FIC0-FM | Yes | Sourced from fabric |
2 | FIC1-FM | Yes | Sourced from fabric |
3 | FIC2-FM | Yes | Sourced from fabric |
4 | Crypto Processor | No | Set by System register, the value is fixed once set |
5 | GEM0 | Yes | Set by Ethernet MAC |
6 | GEM1 | Yes | Set by Ethernet MAC |
7 | USB | No | Set by System register, the value is fixed once set |
8 | MMC | No | Set by System register, the value is fixed once set |
9 | SCB Bridge | Yes | Set in System Controller SCB interface |
10 | CPLEX-D0 | No | Set by System register, the value is fixed once set |
11 | CPLEX-D1 | No | Set by System register, the value is fixed once set |
12 | CPLEX-F0 | No | Set by System register, the value is fixed once set |
13 | CPLEX-F1 | No | Set by System register, the value is fixed once set |
14 | CPLEX-NC | No | Set by System register, the value is fixed once set |
15 | TRACE | Yes | Set by Trace SMB |