Execute in place (XIP) allows a processor to directly boot from the QSPI device rather than moving the SPI content to SRAM before execution. A system Configuration bit (XIP bit in CONTROL register) is used to set the controller in XIP mode.
When QSPI is in XIP mode, all AHB reads simply return the 32-bit data value associated with the requested address. Each access to the QSPI device requires a 3-byte or 4-byte address transfers, a 3-byte IDLE period and 4-byte data transfer. Assuming the SPI clock is ¼ of the AHB clock, then this requires approximately 80 clock cycles per 32-bit read cycle. In XIP mode, data is returned directly to the AHB bus in response to an AHB read, data is not read from the FIFO’s. The QSPI device stays in XIP mode as long as the Xb bit is zero.
In XIP mode, AHB write cycles access the core registers allowing the values to change, although the registers cannot be read when in XIP mode.
In the application, the XIP mode is not enabled at Reset as the CPUs are initially booted by system controller and the boot code can initialize the normal QSPI configuration registers.
To exit XIP mode, the firmware should clear the XIP bit in the CONTROL register, at this time it should not be executing from the QSPI device. When this bit is written to zero, the QSPI core returns to Normal mode and the reads access the core registers.