By default, the iCache, ITIM, and dCache implement SECDED for ECC. ECC is applied at the 32-bit codeword level, with an ECC overhead of 7 bits per codeword. The ECC feature of L1 cache is handled internally, user control is not supported.
When a single-bit error is detected in the ITIM, the error is corrected automatically and written back to the SRAM. When a single-bit error is detected in the L1 instruction cache, the error is corrected automatically and the cache line is flushed. When a single-bit error is detected in the L1 data cache, the data cache automatically implements the following sequence of operations:
1. Corrects the error.
2. Invalidates the cache line.
3. Writes the line back to the next level of the memory hierarchy.
The ECC reporting scheme is same as described in ECC Reporting.