Start Condition | Operation when EPOL = 0 |
Operation when EPOL = 1 |
---|---|---|
None | No hardware control – timer runs when ON =
1 |
Same as EPOL = 0 |
Either ERS Edge | Timer starts at either edge (rising or falling) of ERS | Same as EPOL = 0 |
Rising ERS Edge | Timer starts at rising edge of ERS | Timer starts at falling edge of ERS |
ERS Level-1 | Timer starts at the first clock where ERS has a high level and the Start condition remains asserted as long as the subsequent clocks register a high ERS level. | Timer starts at the first clock where ERS has a low level and the Start condition remains asserted as long as the subsequent clocks register a low ERS level. |
Reset Condition | Operation when EPOL = 0 |
Operation when EPOL = 1 |
---|---|---|
None | No hardware reset | Same as EPOL = 0 |
ERS Level-0 + PR Match | Timer resets at the first clock where ERS has a low level and the Reset condition remains asserted as long as the subsequent clocks register a low ERS level. Level output and RUN bit become false while the Reset condition is active. A PR match condition also triggers a Reset, in which case the timer resets at the next clock after PR match. Level output and RUN bit remain true in this case. |
Timer resets at the first clock where ERS has a high level and the Reset condition remains asserted as long as the subsequent clocks register a high ERS level. Level output and RUN bit become false while the Reset condition is active. A PR match condition also triggers a Reset, in which case the timer resets at the next clock after PR match. Level output and RUN bit remain true in this case. |
At Start + PR Match | Timer resets at the first clock whenever a Start condition is generated. A PR match condition also triggers a Reset, in which case the timer resets at the next clock after PR match. Level output and RUN bit remain true in either case. | Same as EPOL = 0 |
At PR Match | Timer resets at the next clock after a PR match condition is generated. Level output and RUN bit remain true in this case. | Same as EPOL = 0 |
Reset Condition | Operation when EPOL = 0 |
Operation when EPOL = 1 |
---|---|---|
None | No hardware control – timer stops when ON =
0 . Capture occurs at every rising ERS
edge. |
No hardware control – timer stops when ON =
0 . Capture occurs at every falling ERS
edge. |
Either ERS Edge | Timer stops at either edge (rising or falling) of ERS and causes a capture event | Same as EPOL = 0 |
Rising ERS Edge | Timer stops at rising edge of ERS and causes a capture event. | Timer stops at falling edge of ERS and causes a capture event |
At PR Match | Timer stops at the next clock after a PR match condition occurs and causes a capture event. | Same as EPOL = 0 |