Timer Setting | Value |
---|---|
START | None (ON = 1 ) |
RESET | At PR Match |
STOP | None |
CSYNC (Clock Sync) | Sync |
PR (Period Register) | Desired Period Value - 1 (e.g., for a desired period of 20, PR = 19) |
The counter counts until a PR match occurs, and then rolls over to zero and continues counting. At PR match, the PRIF interrupt and output pulse occur. At the following clock, the counter returns to zero and the ZIF interrupt occurs. This is shown in Figure 2-1.
If RESET = None, the counter will rollover at the maximum value of the timer (0xF...FF) with ZIF, but the output pulse and PRIF will occur at PR match. This is shown in Figure 2-2.