8-bit AVR Microcontroller

Status Register

When addressing I/O Registers as data space using LD and ST instructions, the provided offset must be used. When using the I/O specific commands IN and OUT, the offset is reduced by 0x20, resulting in an I/O address offset within 0x00 - 0x3F.

Name:
SREG
Offset:
0x5F
Reset:
0x00
Access:
When addressing as I/O Register: address offset is 0x3F
Bit76543210
ITHSVNZC
AccessR/WR/WR/WR/WR/WR/WR/WR/W
Reset00000000

Bit 7 – I: Global Interrupt Enable

Global Interrupt Enable

The Global Interrupt Enable bit must be set for the interrupts to be enabled. The individual interrupt enable control is then performed in separate control registers. If the Global Interrupt Enable Register is cleared, none of the interrupts are enabled independent of the individual interrupt enable settings. The I-bit is cleared by hardware after an interrupt has occurred, and is set by the RETI instruction to enable subsequent interrupts. The I-bit can also be set and cleared by the application with the SEI and CLI instructions, as described in the instruction set reference.

Bit 6 – T: Copy Storage

Copy Storage

The Bit Copy instructions BLD (Bit LoaD) and BST (Bit STore) use the T-bit as source or destination for the operated bit. A bit from a register in the Register File can be copied into T by the BST instruction, and a bit in T can be copied into a bit in a register in the Register File by the BLD instruction.

Bit 5 – H: Half Carry Flag

Half Carry Flag

The Half Carry Flag H indicates a Half Carry in some arithmetic operations. Half Carry Flag is useful in BCD arithmetic. See the Instruction Set Description for detailed information.

Bit 4 – S: Sign Flag, S = N ㊉ V

Sign Flag, S = N ㊉ V

The S-bit is always an exclusive or between the Negative Flag N and the Two’s Complement Overflow Flag V. See the Instruction Set Description for detailed information.

Bit 3 – V: Two’s Complement Overflow Flag

Two’s Complement Overflow Flag

The Two’s Complement Overflow Flag V supports two’s complement arithmetic. See the Instruction Set Description for detailed information.

Bit 2 – N: Negative Flag

Negative Flag

The Negative Flag N indicates a negative result in an arithmetic or logic operation. See the Instruction Set Description for detailed information.

Bit 1 – Z: Zero Flag

Zero Flag

The Zero Flag Z indicates a zero result in an arithmetic or logic operation. See the Instruction Set Description for detailed information.

Bit 0 – C: Carry Flag

Carry Flag

The Carry Flag C indicates a carry in an arithmetic or logic operation. See the Instruction Set Description for detailed information.