The USB protocol is a master/slave protocol. This is the host that starts the enumeration sending requests to the device through the control endpoint. The device handles standard requests as defined in the USB Specification.
Request | Definition |
---|---|
GET_DESCRIPTOR | Returns the current device configuration value. |
SET_ADDRESS | Sets the device address for all future device access. |
SET_CONFIGURATION | Sets the device configuration. |
GET_CONFIGURATION | Returns the current device configuration value. |
GET_STATUS | Returns status for the specified recipient. |
SET_FEATURE | Set or Enable a specific feature. |
CLEAR_FEATURE | Clear or Disable a specific feature. |
The device also handles some class requests defined in the CDC class.
Request | Definition |
---|---|
SET_LINE_CODING | Configures DTE rate, stop bits, parity and number of character bits. |
GET_LINE_CODING | Requests current DTE rate, stop bits, parity and number of character bits. |
SET_CONTROL_LINE_STATE | RS-232 signal used to tell the DCE device the DTE device is now present. |
Unhandled requests are STALLed.