SMC Mode Register
This register can only be written if the WPEN bit is cleared in the “SMC Write Protection Mode Register”.
The user must confirm the SMC configuration by writing any one of the SMC_MODE registers.
Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
PS[1:0] | PMEN | ||||||||
Access | |||||||||
Reset |
Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
TDF_MODE | TDF_CYCLES[3:0] | ||||||||
Access | |||||||||
Reset |
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
DBW | BAT | ||||||||
Access | |||||||||
Reset |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
EXNW_MODE[1:0] | WRITE_MODE | READ_MODE | |||||||
Access | |||||||||
Reset |
Read Mode
Value | Description |
---|---|
0 | The read operation is controlled by the NCS signal. – If TDF cycles are programmed, the external bus is marked busy after the rising edge of NCS. – If TDF optimization is enabled (TDF_MODE =1), TDF wait states are inserted after the setup of NCS. |
1 | The read operation is controlled by the NRD signal. – If TDF cycles are programmed, the external bus is marked busy after the rising edge of NRD. – If TDF optimization is enabled (TDF_MODE =1), TDF wait states are inserted after the setup of NRD. |
Write Mode
Value | Description |
---|---|
0 | The write operation is controlled by the NCS signal. – If TDF optimization is enabled (TDF_MODE =1), TDF wait states will be inserted after the setup of NCS. |
1 | The write operation is controlled by the NWE signal. – If TDF optimization is enabled (TDF_MODE =1), TDF wait states will be inserted after the setup of NWE. |
NWAIT Mode
The NWAIT signal is used to extend the current read or write signal. It is only taken into account during the pulse phase of the read and write controlling signal. When the use of NWAIT is enabled, at least one cycle hold duration must be programmed for the read and write controlling signal.
Value | Name | Description |
---|---|---|
0 | DISABLED | Disabled–The NWAIT input signal is ignored on the corresponding chip select. |
1 |
Reserved |
|
2 | FROZEN | Frozen Mode–If asserted, the NWAIT signal freezes the current read or write cycle. After deassertion, the read/write cycle is resumed from the point where it was stopped. |
3 | READY | Ready Mode–The NWAIT signal indicates the availability of the external device at the end of the pulse of the controlling read or write signal, to complete the access. If high, the access normally completes. If low, the access is extended until NWAIT returns high. |
Byte Access Type
This field is used only if DBW defines a 16-bit data bus.
Value | Name | Description |
---|---|---|
0 | BYTE_SELECT | Byte select access type: - Write operation is controlled using NCS, NWE, NBS0, NBS1. - Read operation is controlled using NCS, NRD, NBS0, NBS1. |
1 | BYTE_WRITE | Byte write access type: - Write operation is controlled using NCS, NWR0, NWR1. - Read operation is controlled using NCS and NRD. |
Data Bus Width
Value | Name | Description |
---|---|---|
0 | 8_BIT | 8-bit Data Bus |
1 | 16_BIT | 16-bit Data Bus |
Data Float Time
This field gives the integer number of clock cycles required by the external device to release the data after the rising edge of the read controlling signal. The SMC always provide one full cycle of bus turnaround after the TDF_CYCLES period. The external bus cannot be used by another chip select during TDF_CYCLES + 1 cycles. From 0 up to 15 TDF_CYCLES can be set.
TDF Optimization
Value | Description |
---|---|
0 | TDF optimization disabled–the number of TDF wait states is inserted before the next access begins. |
1 | TDF optimization enabled–the number of TDF wait states is optimized using the setup period of the next read/write access. |
Page Mode Enabled
Value | Description |
---|---|
0 | Standard read is applied. |
1 | Asynchronous burst read in page mode is applied on the corresponding chip select. |
Page Size
If page mode is enabled, this field indicates the size of the page in bytes.
Value | Name | Description |
---|---|---|
0 | 4_BYTE | 4-byte page |
1 | 8_BYTE | 8-byte page |
2 | 16_BYTE | 16-byte page |
3 | 32_BYTE | 32-byte page |