The RSTC is made up of an NRST manager and a reset state manager. It runs at SLCK frequency and generates the following reset signals:
These reset signals are asserted by the RSTC, either on events generated by peripherals, events on the NRST pin, or on a software action. The reset state manager controls the generation of reset signals and provides a signal to the NRST manager when an assertion of the NRST pin is required.
The NRST manager shapes the NRST assertion during a programmable time, thus controlling external device resets.
The RSTC Mode register (RSTC_MR), used to configure the RSTC, is powered with VDDIO, so that its configuration is saved as long as VDDIO is on.