The TWIHS can perform a quick command by following these steps:
- 1.Configure the Master mode (DADR, CKDIV, etc).
- 2.Write TWIHS_MMR.MREAD at the value of the one-bit command to be sent.
- 3.Start the transfer by setting TWIHS_CR.QUICK.
Figure 1. SMBus Quick Command