GMAC Length Field Frame Errors Register
|
0x194 |
32 |
- |
0x00000000 |
|
Length Field Frame
Errors
This bit field counts the number of frames
received that have a measured length shorter than that extracted from the length
field (Bytes 13 and 14). This condition is only counted if the value of the length
field is less than 0x0600, the frame is not of excessive length and checking is
enabled by writing a '1' to the Length Field Error Frame Discard bit in the Network
Configuration Register (GMAC_NCFGR.LFERD).