The following algorithm puts the device in Parallel Programming mode:
- 1.Apply the supplies as described in table Signal Description List.
- 2.External clock is applied to the XIN pin
within the VDDCORE POR reset time-out period, as defined in the section “Electrical
Characteristics”.
- 3.Wait for the end of this reset period.
- 4.Start a read or write handshaking.