PWM Channel Mode Register
This register can only be written if bits WPSWS2 and WPHWS2 are cleared in the PWM Write Protection Status Register.
Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
Access | |||||||||
Reset |
Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
PPM | DTLI | DTHI | DTE | ||||||
Access | R/W | R/W | R/W | R/W | |||||
Reset | 0 | 0 | 0 | 0 |
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
TCTS | DPOLI | UPDS | CES | CPOL | CALG | ||||
Access | R/W | R/W | R/W | R/W | R/W | R/W | |||
Reset | 0 | 0 | 0 | 0 | 0 | 0 |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
CPRE[3:0] | |||||||||
Access | R/W | R/W | R/W | R/W | |||||
Reset | 0 | 0 | 0 | 0 |
Channel Prescaler
Value | Name | Description |
---|---|---|
MCK | Peripheral clock |
|
1 | MCK_DIV_2 | Peripheral clock/2 |
2 | MCK_DIV_4 | Peripheral clock/4 |
3 | MCK_DIV_8 | Peripheral clock/8 |
4 | MCK_DIV_16 | Peripheral clock/16 |
5 | MCK_DIV_32 | Peripheral clock/32 |
6 | MCK_DIV_64 | Peripheral clock/64 |
7 | MCK_DIV_128 | Peripheral clock/128 |
8 | MCK_DIV_256 | Peripheral clock/256 |
9 | MCK_DIV_512 | Peripheral clock/512 |
10 | MCK_DIV_1024 | Peripheral clock/1024 |
11 | CLKA | Clock A |
12 | CLKB | Clock B |
Channel Alignment
Value | Description |
---|---|
0 | The period is left-aligned. |
1 | The period is center-aligned. |
Channel Polarity
Value | Description |
---|---|
0 | The OCx output waveform (output from the comparator) starts at a low level. |
1 | The OCx output waveform (output from the comparator) starts at a high level. |
Counter Event Selection
The bit CES defines when the channel counter event occurs when the period is center-aligned (flag CHIDx in PWM Interrupt Status Register 1).
If the PWM period is center-aligned (CALG=1):
0: The channel counter event occurs at the end of the PWM period.
1: The channel counter event occurs at the end of the PWM period and at half the PWM period.
If the PWM period is left-aligned (CALG=0), the channel counter event occurs at the end of the period and the CES bit has no effect.
Update Selection
If the PWM period is center-aligned (CALG=1):
0: The update occurs at the next end of the PWM period after writing the update register(s).
1: The update occurs at the next end of the PWM half period after writing the update register(s).
If the PWM period is left-aligned (CALG=0), the update always occurs at the end of the PWM period after writing the update register(s).
Disabled Polarity Inverted
Value | Description |
---|---|
0 | When the PWM channel x is disabled (CHIDx(PWM_SR) = 0), the OCx output waveform is the same as the one defined by the CPOL bit. |
1 | When the PWM channel x is disabled (CHIDx(PWM_SR) = 0), the OCx output waveform is inverted compared to the one defined by the CPOL bit. |
Timer Counter Trigger Selection
Value | Description |
---|---|
0 | The comparator of the channel x (OCx) is used as the trigger source for the Timer Counter (TC). |
1 | The counter events of the channel x is used as the trigger source for the Timer Counter (TC). |
Dead-Time Generator Enable
Value | Description |
---|---|
0 | The dead-time generator is disabled. |
1 | The dead-time generator is enabled. |
Dead-Time PWMHx Output Inverted
Value | Description |
---|---|
0 | The dead-time PWMHx output is not inverted. |
1 | The dead-time PWMHx output is inverted. |
Dead-Time PWMLx Output Inverted
Value | Description |
---|---|
0 | The dead-time PWMLx output is not inverted. |
1 | The dead-time PWMLx output is inverted. |
Push-Pull Mode
The Push-Pull mode is enabled for channel x.
Value | Description |
---|---|
0 | The Push-Pull mode is disabled for channel x. |
1 | The Push-Pull mode is enabled for channel x. |