MediaLB Interrupt Enable Register
|
0x02C |
32 |
Read/Write |
0x00000000 |
|
Isochronous Rx Protocol Error Enable
Value | Description |
---|
1 |
A ProtocolError detected on an isochronous Rx channel causes the appropriate channel bit in the MLB_MS0 or
MLB_MS1 registers to be set. |
Isochronous Rx Buffer Overflow Enable
Value | Description |
---|
1 |
A buffer overflow on an isochronous Rx channel causes the appropriate channel bit in the MLB_MS0 or MLB_MS1
registers to be set. This occurs only when isochronous flow control is disabled. |
Synchronous Protocol Error Enable
Value | Description |
---|
1 |
A ProtocolError detected on a synchronous Rx channel causes the appropriate channel bit in the MLB_MS0 or
MLB_MS1 registers to be set. |
Asynchronous Rx Done Enable
Value | Description |
---|
1 |
A packet received with no errors on an asynchronous Rx channel causes the appropriate channel bit in the MLB_MS0
or MLB_MS1 registers to be set. |
Asynchronous Rx Protocol Error Enable
Value | Description |
---|
1 |
A ProtocolError detected on an asynchronous Rx channel causes the appropriate channel bit in the MLB_MS0 or
MLB_MS1 registers to be set. |
Asynchronous Rx Break Enable
Value | Description |
---|
1 |
A AsyncBreak command received from the transmitter on an asynchronous Rx channel causes the appropriate channel
bit in the MLB_MS0 or MLB_MS1 registers to be set. |
Asynchronous Tx Packet Done Enable
Tx channel causes the appropriate channel bit in the MLB_MS0 or MLB_MS1 registers to be set.
Value | Description |
---|
1 |
A packet transmitted with no errors on an asynchronous |
Asynchronous Tx Protocol Error Enable
Value | Description |
---|
1 |
A ProtocolError generated by the receiver on an asynchronous Tx channel causes the appropriate channel bit in
the MLB_MS0 or MLB_MS1 registers to be set. |
Asynchronous Tx Break Enable
Value | Description |
---|
1 |
A ReceiverBreak response received from the receiver on an asynchronous Tx channel causes the appropriate channel
bit in the MLB_MS0 or MLB_MS1 registers to be set. |
Control Rx Packet Done Enable
Value | Description |
---|
1 |
A packet received with no errors on a control Rx channel causes the appropriate channel bit in the MLB_MS0 or
MLB_MS1 registers to be set. |
Control Rx Protocol Error Enable
Value | Description |
---|
1 |
A ProtocolError detected on a control Rx channel causes the appropriate channel bit in the MLB_MS0 or MLB_MS1
registers to be set. |
Control Rx Break Enable
Rx channel causes the appropriate channel bit in the MLB_MS0 or MLB_MS1 registers to be set.
Value | Description |
---|
1 |
A ControlBreak command received from the transmitter on a control. |
Control Tx Packet Done Enable
Value | Description |
---|
1 |
A packet transmitted with no errors on a control Tx channel causes the appropriate channel bit in the MLB_MS0 or
MLB_MS1 registers to be set. |
Control Tx Protocol Error Enable
Value | Description |
---|
1 |
A ProtocolError generated by the receiver on a control Tx channel causes the appropriate channel bit in the
MLB_MS0 or MLB_MS1 registers to be set. |