The Flash Write command is used to write the Flash contents.
The Flash memory plane is organized into several pages. Data to be written are stored in a load buffer that corresponds to a Flash memory page. The load buffer is automatically flushed to the Flash:
The Write Page command (WP) is optimized for consecutive writes. Write handshaking can be chained; an internal address buffer is automatically increased. An additional WP command must be executed if a full page is not written or if the write data starts from a non-zero page offset.
Step | Handshake Sequence | MODE[3:0] | DATA[15:0] |
---|---|---|---|
1 | Write handshaking | CMDE | WP or WPL or EWP or EWPL |
2 | Write handshaking | ADDR0 | Memory Address LSB |
3 | Write handshaking | ADDR1 | Memory Address |
4 | Write handshaking | DATA | *Memory Address++ |
5 | Write handshaking | DATA | *Memory Address++ |
... | ... | ... | ... |
n | Write handshaking | ADDR0 | Memory Address LSB |
n+1 | Write handshaking | ADDR1 | Memory Address |
n+2 | Write handshaking | DATA | *Memory Address++ |
n+3 | Write handshaking | DATA | *Memory Address++ |
... | ... | ... | ... |
The Flash command Write Page and Lock (WPL) is equivalent to the Flash Write Command. However, the lock bit is automatically set at the end of the Flash write operation. As a lock region is composed of several pages, the programmer writes to the first pages of the lock region using Flash write commands and writes to the last page of the lock region using a Flash write and lock command.
The Flash command Erase Page and Write (EWP) is equivalent to the Flash Write Command. However, before programming the load buffer, the page is erased.
The Flash command Erase Page and Write the Lock (EWPL) combines EWP and WPL commands.