ISI Write Protection Status Register
|
0xE8 |
32 |
Read-only |
0x00000000 |
|
Write Protection Violation Status
Value | Name |
---|
0 |
No write protection violation occurred since the last read of ISI_WPSR. |
1 |
A write protection violation has occurred since the last read of the ISI_WPSR. If this violation is an unauthorized attempt to write a protected register, the associated violation is reported into field WPVSRC. |
Write Protection Violation Source
Value | Name |
---|
0 |
No Write Protection Violation occurred since the last read of this register (ISI_WPSR). |
1 |
Write access in ISI_CFG1 while Write Protection was enabled (since the last read). |
2 |
Write access in ISI_CFG2 while Write Protection was enabled (since the last read). |
3 |
Write access in ISI_PSIZE while Write Protection was enabled (since the last read). |
4 |
Write access in ISI_PDECF while Write Protection was enabled (since the last read). |
5 |
Write access in ISI_Y2R_SET0 while Write Protection was enabled (since the last read). |
6 |
Write access in ISI_Y2R_SET1 while Write Protection was enabled (since the last read). |
7 |
Write access in ISI_R2Y_SET0 while Write Protection was enabled (since the last read). |
8 |
Write access in ISI_R2Y_SET1 while Write Protection was enabled (since the last read). |
9 |
Write access in ISI_R2Y_SET2 while Write Protection was enabled (since the last read). |