The NCS signal waveforms in write operation are not the same that those applied in read operations, but are separately defined:
- ncs_wr_setup—the NCS setup time is defined as the setup time of address before the NCS falling edge.
- ncs_wr_pulse—the NCS pulse length is the time between NCS falling edge and NCS rising edge;
- ncs_wr_hold—the NCS hold time is defined as the hold time of
address after the NCS rising edge.
Figure 1. Write Cycle