Initialize the AST digital tuner.
void ast_init_digital_tuner( Ast * ast, bool add, uint8_t value, uint8_t exp)
Data direction | Parameter name | Description |
---|---|---|
[in, out] |
ast |
Module hardware register base address pointer |
[in] |
add |
Set to true if the frequency needs to be increased, false if it has to be decreased. |
[in] |
value |
Parameter used in the formula |
[in] |
exp |
Parameter used in the formula |