The following are the steps to add dynamic regional configuration:
- 1.Enable the required regional band configuration in the MLS. For more information on
enabling/disabling the regional band configuration, refer to Building the Firmware.
- 2.Application must call the MAC reset API for every band switching with the required
regional band as a parameter. For the MAC reset API and
inc/stack_common.h
for the regional band enumeration, refer to
API document.