The MLS stack supports multiple regional configurations. It is possible to disable one or more regional configurations at the compile time, but at least one regional configuration must be enabled. MLS also supports run time switching between the supported regional configurations. For the supported regional configuration in the package, refer to the release notes.
The following are the advantages of multiband:
Macro Switch Name | Band(s) Supported |
---|---|
AS_BAND | Brunei, Cambodia, Indonesia, Laos, New Zealand, Singapore, Taiwan, Thailand, Vietnam |
AU_BAND | Australia |
EU_BAND | Europe 868 MHz |
IND_BAND | India |
JPN_BAND | Japan |
KR_BAND | Korea |
NA_BAND | North America |