Perform the following steps to Flash the firmware on the SAM R34 Xplained Pro board or the WLR089 Xplained Pro board.
- 1.After successfully building the
firmware, connect the SAM R34 Xplained Pro board or the
WLR089 Xplained Pro board to the PC through the USB cable. Atmel Studio detects the
board after completing the driver installation.
- 2.Go to
Tools > Device
Programming
or press <Ctrl + Shift + P>.Figure 1. Opening the Device
Programming Window
- 3.The Device Programming window
displays. Perform the following steps:
- 3.1.From the Tool list, select
EDBG ATMLXXXXXXX. This automatically fills the Device field.
Click Apply.
- 3.2.Click Read to read the
Device Signature value.
Figure 2. Selecting the
Debugger
- 3.3.From the left-hand menu list,
click Memories.
- 3.4.In the Flash pane, browse for
the
elf
file, then click Program.Figure 3. Flashing the
Image