int CRYPT_ECC_DHE_SharedSecretMake(
CRYPT_ECC_CTX* priv,
CRYPT_ECC_CTX* pub,
unsigned char* out,
unsigned int outSz,
unsigned int* usedSz
);
This function takes two ECC contexts (one public, one private) and creates a shared secret between the two. The secret conforms to EC-DH from ANSU X9.63.
Both contexts must have been initialized with a call to CRYPT_ECC_Initialize. Both contexts have had their respective keys imported or created.
Parameters | Description |
---|---|
priv | Pointer to the private ECC context (with the private key). |
pub | Pointer to the public ECC context (with the public key). |
out | Destination of the shared secret. |
outSz | The max size of the shared secret. |
usedSz | Resulting size of the shared secret. |
BAD_FUNC_ARG - An invalid pointer was passed to the function.
MEMORY_E - Could not create the memory buffer for the shared secret.
0 - An invalid pointer was not passed to the function.
None.
CRYPT_ECC_CTX userA;
CRYPT_ECC_CTX userB;
int ret;
byte sharedA[100];
unsigned int aSz = (unsigned int)sizeof(sharedA);
unsigned int usedA = 0;
ret = CRYPT_ECC_Initialize(&userA);
ret = CRYPT_ECC_Initialize(&userB);
...
// Make or import the appropriate keys
...
ret = CRYPT_ECC_DHE_SharedSecretMake(&userA, &userB, sharedA, aSz, &usedA);