int CRYPT_ECC_SignatureSizeGet(
CRYPT_ECC_CTX* ecc
);
This function returns the size of the signature in a given context, in octets.
The ECC context must have been initialized with a call to CRYPT_ECC_Initialize. The keys must have been imported or created prior to calling this function.
Parameters | Description |
---|---|
ecc | Pointer to context which saves state between calls, and contains the signature. |
BAD_FUNC_ARG - An invalid pointer was passed to the function.
int - The size of the signature.
None.
CRYPT_ECC_CTX userA;
int ret;
byte sig[100];
unsigned int sigSz = (unsigned int)sizeof(sig);
unsigned int usedA = 0;
ret = CRYPT_ECC_Initialize(&userA);
...
// Import or generate private key
...
ret = CRYPT_ECC_SignatureSizeGet(&userA);