int CRYPT_SHA_Initialize(
CRYPT_SHA_CTX* sha
);
This function initializes the internal structures necessary for SHA hash calculations.
None.
Parameters | Description |
---|---|
sha | Pointer to CRYPT_SHA_CTX structure which holds the hash values. |
BAD_FUNC_ARG - An invalid pointer was passed to the function.
0 - An invalid pointer was not passed to the function.
All SHA hashes have to start at a particular value before adding new data to it. Thus function sets the necessary values for the structure.
CRYPT_SHA_CTX sha;
uint8_t shaSum[SHA_DIGEST_SIZE];
CRYPT_SHA_Initialize(&sha);
CRYPT_SHA_DataAdd(&sha, buffer, sizeof(buffer));
CRYPT_SHA_Finalize(&sha, shaSum);