int CRYPT_SHA256_Initialize(
CRYPT_SHA256_CTX* sha256
);
This function initializes the internal structures necessary for SHA256 hash calculations.
None.
Parameters | Description |
---|---|
sha256 | Pointer to context which saves state between calls. |
BAD_FUNC_ARG - An invalid pointer was passed to the function.
0 - An invalid pointer was not passed to the function.
All SHA hashes have to start at a particular value before adding new data to it. This function sets the necessary values for the structure.
CRYPT_SHA256_CTX sha;
uint8_t shaSum[SHA256_DIGEST_SIZE];
CRYPT_SHA256_Initialize(&sha);
CRYPT_SHA256_DataAdd(&sha, buffer, sizeof(buffer));
CRYPT_SHA256_Finalize(&sha, shaSum);