int CRYPT_ECC_PublicExport(
CRYPT_ECC_CTX* ecc,
unsigned char* out,
unsigned int outSz,
unsigned int* usedSz
);
This function takes an ECC public key and exports it in ANSI X9.63 format.
The context must be initialized previously with a call to CRYPT_ECC_Initialize. The key must also have been constructed with a call to CRYPT_ECC_DHE_KeyMake. A random number generator must have been initialized with a call to CRYPT_RNG_Initialize.
Parameters | Description |
---|---|
ecc | Pointer to context which saves state between calls. |
out | Buffer in which to store the public key. |
outSz | The available size of the buffer, in bytes. |
usedSz | Return value indicating how many bytes were used. |
BAD_FUNC_ARG - An invalid pointer was passed to the function.
BUFFER_E - The output buffer was too small to store the key.
0 - An invalid ppointer was not passed to the function.
None.
CRYPT_ECC_CTX userA;
int ret;
byte sharedA[100];
unsigned int aSz = (unsigned int)sizeof(sharedA);
unsigned int usedA = 0;
ret = CRYPT_ECC_Initialize(&userA);
ret = CRYPT_ECC_DHE_KeyMake(&userA, &mcRng, 32);
ret = CRYPT_ECC_PublicExport(&userA, sharedA, aSz, &usedA);