int CRYPT_AES_GCM_Decrypt(
CRYPT_AES_CTX* aes,
unsigned char* out,
const unsigned char* in,
unsigned int sz,
const unsigned char* iv,
unsigned int ivSz,
const unsigned char* authTag,
unsigned int authTagSz,
const unsigned char* authIn,
unsigned int authInSz
);
This function decrypts a block of data using the AES algorithm in Galois/Counter Mode (GCM).
Key must be set earlier with a call to CRYPT_AES_GCM_SetKey.
Parameters | Description |
---|---|
aes | Pointer to context which saves state between calls. |
out | Pointer to buffer to store the results of the decryption pass. |
in | Pointer to buffer holding the data to be decrypted. |
sz | Size of the input data, in bytes. |
iv | Pointer to the initialization vector. |
ivSz | Size of the initialization vector. |
authTag | Pointer to the buffer to store the authentication tag. |
authTagSz | Size of the authentication tag. |
authIn | Pointer to the additional authentication data. |
authInSz | Size of the additional authentication data. |
BAD_FUNC_ARG - An invalid pointer was passed to the function. -AES_GCM_AUTH_E - The authTag is incorrect.
0 - An invalid pointer was not passed to the function.
The output buffer must be equal in size to the input buffer.