“Code Coverage” selections are:
- If “Disable” is selected, code coverage is disabled and its options are not
available.
- If “Enabled/Reset on POR” is selected, code coverage is reset when power-on reset is
applied.
- If “Enabled/Reset on Run” is selected, code coverage is reset every time run is
executed within the simulator.
When a reset has occurred, and simulation has run and then paused, a report will be shown
in the Output window, Debugger Console tab, or Output file, depending on options
chosen.
Figure 1. Simulator Code Coverage
Output
All executed program memory locations will be shown as ranges. Click on
the links to go to the first or last line of the code that was covered.
Figure 2. Simulator Code Coverage
Links