The code examples are available through Atmel START, which is a web-based tool that enables the configuration of the application code through a Graphical User Interface (GUI). The code can be downloaded for Atmel Studio, MPLAB® X and IAR Embedded Workbench® via the direct example code link below or the Browse Examples button on the Atmel START front page.
The Atmel START webpage can be found here: Atmel START.
Code Examples
Finding code examples for devices in the tinyAVR 2 Family can be done by searching for the device name (e.g., ATtiny1627), in the Atmel START example browser.
Click User Guide in Atmel START for details and information about example projects. The User Guide button can be found in the example browser and by clicking the project name in the dashboard view within the Atmel START project configurator.
Microchip Studio/Atmel Studio
Download the code as a .atzip
file for Microchip Studio/Atmel Studio
from the example browser in Atmel START by clicking Download Selected example. To
download the file from within Atmel START, click Export project followed by
Download pack.
Double click the downloaded .atzip
file, and the project will be
imported to Microchip Studio/Atmel Studio 7.0
MPLAB® X
Download the code as a .atzip
file for MPLAB X IDE from within Atmel
START by clicking Export project followed by Download pack.
To open the Atmel START example in MPLAB X, select from the menu in MPLAB X,
.atzip
file.
IAR Embedded Workbench®
For information on how to import the project in IAR Embedded Workbench, open the Atmel START User Guide, select Using Atmel Start Output in External Tools, and IAR Embedded Workbench. A link to an online version of the Atmel START User Guide can be found by clicking Help from the Atmel START front page or Help And Support within the project configurator, both located in the upper right corner of the page.