The code examples are available through GitHub, which is a web-based server that provides
the application codes through a Graphical User Interface (GUI). The code examples can be
opened in both Microchip Studio and MPLAB X. To open the Microchip Studio project in
MPLAB X, select from the menu, .cproj
file.
The GitHub webpage: GitHub.
Code Examples
Finding code examples for devices in the tinyAVR 2 Family can be done by searching for the device name (e.g., ATtiny1627), in the GitHub example browser.
Download the code as a .zip
file from the example page on
GitHub by clicking the Clone or download button.