The plane under the pads of DC blocking capacitors must be removed (as shown in the following
figure) to match the impedance of the pad to 50 Ω.
Note: This has to be performed only on
immediate reference plane and not on all planes.
Figure 1. Capacitor Pad Reference Plane