Qualification of simulation results is based on the eye-height, eye-width, and BER curves. Check the eye-height and eye-width at target BER of 10e-12. These results are found in the report generated by the simulation tool. For example, the Sigrity tool gives the following information at RX:
At BER of 10e-12, running at 5 Gbps bit rate
This simulation is on the SmartFusion2 Development Kit using the Sigrity tool and the waveforms are shown in the following figure. The simulation result shows that it meets the PCIe 2.0 requirements.
The following table lists the specifications of the received signal for PCIe.
Bit Rate |
Min Height of the Eye at RX |
Min Width of the Eye at RX |
---|---|---|
2.5 Gbps |
175 mV |
0.6 UI |
5 Gbps |
120 mV |
0.6 UI |
For more information about PCIe 2.0 base specification, see www.pcisig.com/members/downloads/specifications/pciexpress/PCI_Express_Base_r2_1_04Mar09.pdf.
To know if the system is meeting the requirements, the eye mask can be imported. Specifications of eye mask depend on the application the system is using. For example, PCIe 1.0, PCIe 2.0, XAUI, and SGMII. A typical eye mask for PCIe 2.0 is shown in the following figure.
For more information about IBIS-AMI model, see AC292- IBIS Models- Background and Usage Application Note.