I/O glitches can occur in some power-down sequences, and they can be ignored if good design
practices are used.
To mitigate the I/O glitch:
- 1.Use any one of the following power-down
sequence:
- a.Ensure that the DEVRST_N is kept
de-asserted at 3.3 V while the power down of all the rails take place. DEVRST_N be
asserted to 0 V only after all the rails are powered down.
- b.If possible, place the device in F*F
mode prior to power-down. This also mitigates the glitches even if the DEVRSTn is
asserted first or VPP is powered down first.
- 2.If power sequencing is not possible, add
a 1 KΩ resistor to ground on all critical signal outputs like clocks and resets and other
glitch sensitive I/Os.