Set Position Decoder lower threshold.
int32_t pdec_async_set_low_threshold( struct pdec_async_descriptor *const descr, const uint32_t low_threshold, uint8_t axis )
This function sets Position Decoder lower threshold.
Type: struct pdec_async_descriptor Struct *const
The pointer to the Position Decoder descriptor
Type: const uint32_t
A lower threshold to set
Type: uint8_t
The axis number to set
Type: int32_t
Status of the Position Decoder lower threshold setting.