Displays character string string.
int32_t slcd_sync_write_string( struct slcd_sync_descriptor *const descr, uint8_t *const str, uint32_t len, uint32_t index )
Type: struct slcd_sync_descriptor Struct *const
SLCD descriptor
Type: uint8_t *const
String to be displayed, 0 will turn off the corresponding char to display
Type: uint32_t
Length of the string array
Type: uint32_t
Index of the character Mapping Group
Type: int32_t