Check if conversion is complete.
int32_t adc_async_is_channel_conversion_complete( const struct adc_async_descriptor *const descr, const uint8_t channel )
This function checks if the ADC has finished the conversion.
Type: const struct adc_async_descriptor Struct *const
The pointer to the ADC descriptor
Type: const uint8_t
Channel number
Type: int32_t
The status of the ADC conversion completion checking.
The conversion is complete
The conversion is not complete