Set the required layer position.
static int32_t lcd_set_position( uint8_t layer, int32_t x, int32_t y )
This function set the required layer position.
Type: uint8_t
Index of layer, 0 for base layer.
Type: int32_t
Physical X-position to be used to set up the layer position.
Type: int32_t
Physical Y-position to be used to set up the layer position.
Type: int32_t
Set status.