Send a command on the selected slot.
bool mci_os_send_cmd( struct mci_os_desc *const desc, uint32_t cmd, uint32_t arg )
Type: struct mci_os_desc Struct *const
Mci os descriptor
Type: uint32_t
Command definition
Type: uint32_t
Argument of the command
Type: bool
true if success, otherwise false