The driver is intended for using the SPI master functions in a Real-Time operating system, i.e. is thread safe.
The transfer functions of the SPI Master RTOS driver are optimized for RTOS support. When data transfer is in progress, the transfer functions use semaphore to block the current task or thread until the transfer ends. So the transfer functions do not work without RTOS as the transfer functions must be called in an RTOS task or thread.
During data transfer, the SPI transfer process is not protected, so that a more flexible way can be chosen in application.
Initialize and deinitialize the driver and associated hardware
Register I/O descriptor
Enable or disable SPI master
Hookup callback handlers on read/write/transfer complete, or error events
Read/Write message to/from the slave
Select character size
Set SPI baudrate
Which clock source is used
After the SPI hardware initialization, the spi_m_os_get_io_descriptor function is needed to register an I/O descriptor. Then control the slave select (SS) pin, and start the read/write operation.
The slave select (SS) is not automatically inserted during read/write/transfer, user must use I/O to control the devices' SS.
While read/write/transfer is in progress, the data buffer used must be kept unchanged.
The following shows a simple example of using the SPI master. The SPI master must have been initialized by spi_m_os_init. This initialization will configure the operation of the SPI master.
/**
* Example task of using SPI_0 to echo using the I/O abstraction.
*/
void SPI_0_example_task(void *p)
{
struct io_descriptor *io;
uint16_t data;
(void)p;
spi_m_os_get_io_descriptor(&SPI_0, &io);
/* Control the slave select (SS) pin */
//gpio_set_pin_level(SPI_0_SS, false);
for (;;) {
if (io_read(io, (uint8_t *)&data, 2) == 2) {
/* read OK, handle data. */;
} else {
/* error. */;
}
}
}
#define TASK_TRANSFER_STACK_SIZE ( 256/sizeof( portSTACK_TYPE ))
#define TASK_TRANSFER_STACK_PRIORITY ( tskIDLE_PRIORITY + 0 )
static TaskHandle_t xCreatedTransferTask;
static void task_transfer_create(void)
{
/* Create the task that handles the CLI. */
if (xTaskCreate(SPI_0_example_task, "transfer", TASK_TRANSFER_STACK_SIZE, NULL,
TASK_TRANSFER_STACK_PRIORITY, &xCreatedTransferTask) != pdPASS) {
while(1) {;
}
}
}
static void tasks_run(void)
{
vTaskStartScheduler();
}
int main(void)
{
/* Initializes MCU, drivers and middleware */
atmel_start_init();
task_transfer_create();
tasks_run();
/* Replace with your application code */
while (1) {
}
}
The SPI master peripheral and its related I/O lines and clocks
The NVIC must be configured so that SPI interrupt requests are periodically serviced
RTOS