Removes the list element.
bool list_delete_element( struct list_descriptor *const list, const void *const element )
Type: struct list_descriptor Struct *const
The pointer to a list
Type: const void *const
An element to remove
Type: bool
The result of element removing
The given element is removed from the given list
The given element is not an element of the given list