Set the Word Select pulse Length of the I2S Controller.
int32_t i2s_c_sync_set_ws_length( struct i2s_c_sync_desc * i2s, const uint16_t n_sck )
Note that it works only when the I2S Controller is disabled.
Type: struct i2s_c_sync_desc Struct *
Pointer to the I2S Controller instance.
Type: const uint16_t
Describes how many SCK bits generates a Word Select pulse.
Type: int32_t
Operation status.
Success.
Error.